Hi All RTOS gurus
I'm new to TiRTOS but not new to MCU's.
I recently got my hands on the TiRTOS and we did a board layout that works with the sample code in the TiRTOS cc13xx portfolio. I
I went through the training (online video) by Eric Willburr. I'm gald I did
I'm now busy to wrap my head around the way the RTOS runs a task in idle mode.
Here is what I'm trying to do.
1) I used the led toggle sample that runs a stask every so often
here the code of my main
/*
* ======== empty_min.c ========
*/
/* XDCtools Header files */
#include <xdc/std.h>
#include <xdc/runtime/System.h>
/* BIOS Header files */
#include <ti/sysbios/BIOS.h>
#include <ti/sysbios/knl/Task.h>
#include <ti/sysbios/knl/Clock.h>
/* TI-RTOS Header files */
// #include <ti/drivers/I2C.h>
#include <ti/drivers/PIN.h>
// #include <ti/drivers/SPI.h>
// #include <ti/drivers/UART.h>
// #include <ti/drivers/Watchdog.h>
/* Board Header files */
#include "Board.h"
#define TASKSTACKSIZE 512
Task_Struct task0Struct;
Char task0Stack[TASKSTACKSIZE];
/* Pin driver handle */
static PIN_Handle ledPinHandle;
static PIN_State ledPinState;
/*
* Application LED pin configuration table:
* - All LEDs board LEDs are off.
*/
PIN_Config ledPinTable[] = {
Board_LED0 | PIN_GPIO_OUTPUT_EN | PIN_GPIO_LOW | PIN_PUSHPULL | PIN_DRVSTR_MAX,
Board_LED1 | PIN_GPIO_OUTPUT_EN | PIN_GPIO_LOW | PIN_PUSHPULL | PIN_DRVSTR_MAX,
Board_LED2 | PIN_GPIO_OUTPUT_EN | PIN_GPIO_LOW | PIN_PUSHPULL | PIN_DRVSTR_MAX,
PIN_TERMINATE
};
/*
* ======== heartBeatFxn ========
* Toggle the Board_LED0. The Task_sleep is determined by arg0 which
* is configured for the heartBeat Task instance.
*/
Void heartBeatFxn(UArg arg0, UArg arg1)
{
while (1) {
Task_sleep((UInt)arg0);
PIN_setOutputValue(ledPinHandle, Board_LED0,
!PIN_getOutputValue(Board_LED0));
}
}
Void benSeTask(void)
{
//while(1)
{
unsigned int t,x;
for(t=0;t<500000;t++)
{
x=x++;
}
PIN_setOutputValue(ledPinHandle, Board_LED2,
!PIN_getOutputValue(Board_LED2));
}
}
/*
* ======== main ========
*/
int main(void)
{
Task_Params taskParams;
/* Call board init functions */
Board_initGeneral();
// Board_initI2C();
// Board_initSPI();
// Board_initUART();
// Board_initWatchdog();
/* Construct heartBeat Task thread */
Task_Params_init(&taskParams);
taskParams.arg0 = 1000000 / Clock_tickPeriod;
taskParams.stackSize = TASKSTACKSIZE;
taskParams.stack = &task0Stack;
Task_construct(&task0Struct, (Task_FuncPtr)heartBeatFxn, &taskParams, NULL);
/* Open LED pins */
ledPinHandle = PIN_open(&ledPinState, ledPinTable);
if(!ledPinHandle) {
System_abort("Error initializing board LED pins\n");
}
PIN_setOutputValue(ledPinHandle, Board_LED1, 1);
/* Start BIOS */
BIOS_start();
return (0);
}
I have add the "idle" task as in picture
In the .cfg script I have done this
If I run the application the Led Task is running but the idle loop function does not work as expected.
I would expect that when the Led Task is running the idle loop function must stop and when the Led task is complete that the idle loop function toggles the other led.
So what do I miss?
Kind regards
Ben