Other Parts Discussed in Thread: AM3351
Hi champs,
We are using TI's AM335x SDK v2.00.01.07. Due to cost and memory constraints, we are using the base file system (<SDK/filesystem/arago-base-tisdk-image-am335x-evm.tar.gz). We need QT support in the filesystem as we are using an LCD in our application.
I came across this link - 
Following are my questions:
1) AM3351 does not have graphics accelerator - what changes do we have to do to the default TI settings. For instance, we have disabled SGX in the DTS. Do we need to do anything else?
2) What is the correct way to add QT support to the base file system? We tried adding all library dependencies based on errors reported while executing but could not resolve this particular one - " application failed to start because it could not find or load the Qt platform plugin eglfs" and many such errors.
3) If we have to make our own filesystem, can TI provide the recipe for the base filesystem so that we create ours by adding QT support to it? We have never worked with Yocto or OE - any help in this regard would be highly useful for us.
Thanks!
Regards,
Shashank