This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

USB ASIO interface



Hello, 

I have a project need to make a USB ASIO interface for audio signal capture and generation. Requirements as below. Any suggestion will be appreciated.

1. At least 2 input and 2 output, 8 in and 8 out is also welcome. IIS or SPDIF both OK. 

2. USB interface. 

3. One to two chip solution, easy to use is welcome. Maybe a codec plus a AD/DA chip? 

4. SNR for the AD/DA at least 110dB per channel. 

Thanks. 

Alvis