Other Parts Discussed in Thread: OMAPL138
Hi, all
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, all
I've a OMAPL138 + NAND, my ubl, bootloader, kernel and rootfs are on the NAND.
The TI said :
0xc0700000 uImage
0xc11800000 0x200000 0x400000 rootfs
Question1:Does it mean when linux system booted, the uImage is load to 0xc070000, and the rootfs is loaded to 0xc1180000
Question2: If the rootfs is too large, does it load the entire rootfs still ?
~~~~~~~~~~~~~~~~
In the linux-kernel said,
x000000000000-0x000000020000 : "u-boot env" 128k
0x000000020000-0x000000040000 : "UBL" 128k
0x000000040000-0x0000000c0000 : "u-boot" 512k
0x000000200000-0x000000600000 : "kernel" 4m
0x000000600000-0x000040000000 : "filesystem" 1018m
In the Nand flash_writer said.
if (armubl == 1)
{
gNandBoot.magicNum = UBL_MAGIC_BIN_IMG
gNandBoot.block = 2
gNandBoot.entryPoint = 0x80000000;
gNandBoot.ldAddress = 0x80000000;
}
else if (uboot == 1)
{
gNandBoot.magicNum = UBL_MAGIC_DMA;
gNandBoot.block = 2;
gNandBoot.entryPoint = 0xc1080000;
gNandBoot.ldAddress = 0xc1080000;
Question 3: What does u-boot env" mean?
Question 4: the UBL block and UBOOT block are all 2 in the "nand-flash-writer", but they have different address in NAND-partions, why?
Question5: 0x80000000 is used for UBL but the DSP-Arm-shared_mem alse use this address, why?
Thank you
Hi,
I will try to answer your question as much as I can.
Question1:Does it mean when
linux system booted, the uImage is load to 0xc070000, and the rootfs is
loaded to 0xc1180000 Answer: Yes. Question2:
If the rootfs is too large, does it load the entire rootfs still ? Answer: in this case, the rootfs is a ramdisk. So it is not supposed to be too large to be accommodated in DDR.
Question
3: What does u-boot env" mean? Answer: it means the environment/configuration parameters to be processed by U-Boot, i.e. "bootcmd = ...", "bootargs = ..." etc. They will need to be stored too. Question 4: the UBL block and
UBOOT block are all 2 in the "nand-flash-writer", but they have
different address in NAND-partions, why? Answer: I don't have an answer right now. I will check and answer you back. Question5: 0x80000000 is used
for UBL but the DSP-Arm-shared_mem alse use this address, why? Answer: it means UBL is using this shared memory as temporary buffer. After the UBL completes, the application can use it.