Friends,
I would like to buy the TMS320VC55055 Medical Evaluation kit (EVM) to do basic reasearch. The kit has to be attached to VC5505 EVM to which the data can be displayed on small display or sent to PC. Within the board is rs232 port where it can be connected to PC.
I would like to connect the output of this port to the PC then try to read the data (the data is ECG signals being collected from ECG board via VC5505 EVM) into a Matlab software where I can do further analysis. Matlab allows me to create serial port object (e.g. Out = serial ('COM1');) but I am still not sure whether I can read data from rs232 port or not. My question please, can I get the data out of the rs-232 and fetch it into Matlab.Will Matlab recognise the ECG points? Note: the link below is about the evaluation kit http://focus.tij.co.jp/jp/lit/an/sprab36a/sprab36a.pdf Your feedback is highly appreciated Faisal