Hello,
AM57xx datasheet GPMC section says "Total GPMC load on any signal at 3.3V must not exceed 10pF".
I think this max load capacitance cutoff is less? Is it the I/Os drive strength restricting this?
In our design one NAND Falsh and two FPGAs are on GPMC. Flash has max 10pF and each FPGA has 7pF , so total max 24pF load.
Is the GPMC works at any lower frequency on 3.3V?
Moving to 1.8V GPMC is difficult in our application.
Please provide a working solution for GPMC 3.3V.
Regards,
Srinivas J