This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Execute mkfs.ext3 failed on DM8148



Hi,

I am using a DM8148 evm with  linux 2.6.37, I want to format the emmc device but failed.

I am using 4GB emmc.

root@dm814x-evm:~# mkfs.ext3 -j -L "rootfs" /dev/mmcblk1p2
mke2fs 1.41.14 (22-Dec-2010)
Filesystem label=rootfs
OS type: Linux
Block size=4096 (log=2)
Fragment size=4096 (log=2)
Stride=0 blocks, Stripe width=0 blocks
200000 inodes, 800000 blocks
40000 blocks (5.00%) reserved for the super user
First data block=0
Maximum filesystem blocks=822083584
25 block groups
32768 blocks per group, 32768 fragments per group
8000 inodes per group
Superblock backups stored on blocks:
32768, 98304, 163840, 229376, 294912

Writing inode tables: [ 299.710000] Kernel panic - not syncing: Attempted to kill init!
[ 299.710000] Backtrace:
[ 299.710000] [<c0050bf4>] (dump_backtrace+0x0/0x110) from [<c03f3574>] (dump_stack+0x18/0x1c)
[ 299.720000] r7:d6438000 r6:d6438000 r5:d643bee0 r4:c059af90
[ 299.730000] [<c03f355c>] (dump_stack+0x0/0x1c) from [<c03f35d8>] (panic+0x60/0x17c)
[ 299.740000] [<c03f3578>] (panic+0x0/0x17c) from [<c007ac7c>] (do_exit+0x74/0x5e4)
[ 299.750000] r3:c056a05c r2:d643be20 r1:d64380fc r0:c04d292f
[ 299.750000] [<c007ac08>] (do_exit+0x0/0x5e4) from [<c007b270>] (do_group_exit+0x84/0xb4)
[ 299.760000] [<c007b1ec>] (do_group_exit+0x0/0xb4) from [<c0086304>] (get_signal_to_deliver+0x2d4/0x304)
[ 299.770000] r5:d643bee0 r4:0000000b
[ 299.770000] [<c0086030>] (get_signal_to_deliver+0x0/0x304) from [<c004fa78>] (do_notify_resume+0x7c/0x654)
[ 299.780000] [<c004f9fc>] (do_notify_resume+0x0/0x654) from [<c004ce58>] (work_pending+0x24/0x28)