Other Parts Discussed in Thread: AM3358
Hello All,
I am trying to boot my sitara AM3358 starter kit using winbond 64MB SPI Flash. Till now I have successfully configured the SPI flash with my board and I could easily program this SPI flash using flash writer code available in starterware. The Problem is I am unable to bootload the code using this external SPI. Is it possible to bootload AM3358 StarterKit directly from SPI(without using Altera CPLD). If yes then can somebody please direct me, how to make its boot.bin file. I am using "gpioCardDetect" application as an example.
Regards
Ahmed