Other Parts Discussed in Thread: OMAPL138
Hi,Guys:
we have a ADI's BF609 platform used many years, Now we have a project 2D barcode camera which based on BF609 platform;
We wants to use OMAPL138 to handle graphic and vision processing, system structure shown below:
input: black & white 2D barcode
sensor: CCD
resolution: 240 X 320
processor: OMAPL138
processing speed: 15 mS / Frame (BF609 can reach 150mS/Frame in current stage)
interface:
OMAPL138 Uart for master communication
Ethernet port for debugging which development tools chain
OPEN VC: we need a OPEN VC package which can run on C674X cell
Now, My question is :
1) Does the OMAPL138 can reach 15mS/Frame decoding speed?
2) How can we got the OPEN VC package which can run on C674X platform , Are there any guide or AN for this issues;
Thanks
RZ