Other Parts Discussed in Thread: TCI6638K2K
Hi experts,
My setup:
Board: EVMK2H
MCSDK: MCSDK_bios_3_01_04_07
Seriously, there are some reasons to our leader decides using DSP only boot. First, we have some legacy code of DSP. Second, the important cause is that the rest share memory of our EVMK2H are not enough to implement Arm+Linux Boot.Third,6638K2K can support DSP only Boot according the document, SPRS836D— TCI6638K2K 8.1.2 Boot Modes Supported.
We want to implement DSP only boot using flash memory. You can tell me if we can only use RBL to implement DSP flash boot or do we need to use the IBL? Do the NOR flash and the NAND flash all achieve our need?
Thanks!
Regards,
Brian