Other Parts Discussed in Thread: XIO2001
Hi...
we see a confusing behaviour of the PCI reset pin PRSTn on our custom DM647board. If the PRSTn is asserted (logic 0) we don’t have access to the DSP over JTAG any more. POR and RESET are deassertet (logic 1).
This is contrary to the spruel4b PCI user guide p17: “The PRST pin is the main PCI hardware reset. This resets most of the PCI logic within the external PCI clock domain. This reset brings PCI-specific registers, sequencers, and signals to a consistent state.” p18: “PRSTz: Entire chip minus on-chip emulation logic is reset”. Also in the DM647 manual (sprs372f) (p84): "...does not reset the test and emulation circuit..."
Practically we see that the entire chip PLUS on-chip emulation logic is reset. Do you have any explanation? Is there a way to connect to DM647 via Jtag with PRST asserted?
bye,
Thomas