Other Parts Discussed in Thread: ALP
I used below codes to test the SWOSD_TI_DMA_Fast2D2D() function. the Idea is to regroup 1000,000 shorts into blocks of 1024 shorts. In every 10 shorts, I'll take out 1 short to form a new block. I used 4 DMA channels to transfer data from testData to the 4 buffers in pOn_chip_data[i]; after each transfer, I check the data validity by comparing each short between source and dest. Then I found only the first 4 transfers are valid, then the following transfers will not succeed(none of the1024 shorts in dest are updated ).
----------------------codes in below----------------------------------------
testData = (unsigned short*) malloc(100000*10*sizeof(unsigned short));
assert(testData!=NULL);
for(int i = 0; i < 100000*10; i++){
testData[i] = (i/10)%65536;
}
... ...
#define BLK_SIZE 1024
int tranxCount = 1000000/BLK_SIZE;
unsigned short* restrict pOn_chip_data[4];
//ping-pong buffer;
pOn_chip_data [0]= (unsigned short*)pIdxConst;
pOn_chip_data [1] =(unsigned short*) (pIdxConst+ BLK_SIZE*sizeof(unsigned short));
pOn_chip_data [2] =(unsigned short*) (pIdxConst + 2*BLK_SIZE*sizeof(unsigned short));
pOn_chip_data [3] =(unsigned short*) (pIdxConst + 3*BLK_SIZE*sizeof(unsigned short));
int DmaId[4];
DmaId[0] = TLD_DMA_CH_IN_A;
DmaId[1] = TLD_DMA_CH_IN_B;
DmaId[2] = TLD_DMA_CH_ALP;
DmaId[3] = TLD_DMA_CH_OUT;
for(int dmaId = TLD_DMA_CH_IN_A; dmaId <TLD_DMA_CH_AUX; dmaId++)
{
ECPY_activate(g_HW_obj->ecpyHandle[dmaId]);
}
//1. just loop for the 10 structs
for(t=0; t < 10; t++){
//1.1 take 2 bytes from every 20 bytes in testData,and form an array of BLK_SIZE
for(count = 0; count < tranxCount; count ++){
blkIdx = count*BLK_SIZE;
int dma_Id = DmaId[count%4];
SWOSD_TI_DMA_Fast2D2D( &g_HW_obj->dmaHandle,
dma_Id,
&testData[blkIdx*10+t],
TLDDIRADD(pOn_chip_data[count%4]),
sizeof(unsigned short),
BLK_SIZE,
10*sizeof(unsigned short),
sizeof(unsigned short));
Vps_printf("%s, %d, dma2dcpy, enter,",__FUNCTION__,__LINE__);
SWOSD_TI_DMA_FastWait(&g_HW_obj->dmaHandle);
// check data validity
if(CompareConfidence){
for(int n=0; n < BLK_SIZE; n ++){
if((pOn_chip_data[count%4][n]) != testData[(blkIdx+n)*10+t ]){
if(last_t != t || lastIdx!= blkIdx){
if(last_t >= 0){
Vps_printf("%s, %d, round(%d) on-chip has %d mismatchs in testData idx(%d), t(%d)",
__FUNCTION__,__LINE__, printtRound, errCount, lastIdx, last_t);
}
last_t = t;
lastIdx = blkIdx;
errCount = 0;
}
errCount ++;
if(errCount < 10){
Vps_printf("%s, %d, err in-chip %x != %x, [count%4=%d, n=%d, blkIdx=%d, t=%d, dmaId=%d]",
__FUNCTION__,__LINE__, *((unsigned short*)TLDDIRADD(&pOn_chip_data[count%4][n])), testData[(blkIdx+n)*10+t] ,
count%4,n,blkIdx, t ,DmaId[count%4]);
}
}
}
}
}
for(int dmaId = TLD_DMA_CH_IN_A; dmaId <TLD_DMA_CH_AUX; dmaId++)
{
ECPY_deactivate(g_pTLD_HW_obj->ecpyHandle[dmaId]);
}