Other Parts Discussed in Thread: AM1808
Hi everyone,
Has anyone else had any issues with getting their demo images to run on their AM1808 EVM?
After roughly 20 seconds of booting into the demo application (i.e.: using the LCD touchscreen) the board stops responding. What I mean is that the LCD goes blank, telnet stops responding and nothing is printed out over the UART console anymore.
Every so often I even see kernel errors like:
FATAL: Error inserting minix (/lib/modules/2.6.33-rc4/kernel/fs/minix/minix.ko): Invalid module format
or
Internal error: Oops - undefined instruction: 0 [#1] PREEMPT
amongst a few others.
I tried the SDK version 1_10_00_00 (DaVinci-PSP-SDK-03.20.00.11), SDK version 1_10_00_01 (DaVinci-PSP-SDK-03.20.00.12), re-compiling the kernel myself, and both NAND and SPI boot modes.
If anyone has a suggestion to investigate the problem it would be much appreciated.
Thanks,
Philipp