I'm trying to boot Linux Automotive on an EVM5777G-03-20-00. I can boot the kernel fine, but I cannot get the 10.1" display working.
Which dtb should I be using for this hardware to enable the display+touch controller, and how do I override the default dtb?
Is SW5 USERCONFIG documented somewhere?
Is SYSBOOT 0-15 documented anywhere?
Thanks,
Joel