This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Which source tree for building Keystone2 Linux?

Please advise which git tree I should download to build Linux for the Keystone 2.  I downloaded from git.ti.com/.../linux today but make uImage fails as I show below:

john@ubuntu64:/opt/keystone-linux-linux$ make uImage

CHK include/generated/uapi/linux/version.h
UPD include/generated/uapi/linux/version.h
CHK include/generated/utsrelease.h
UPD include/generated/utsrelease.h
Generating include/generated/mach-types.h
CC kernel/bounds.s
GEN include/generated/bounds.h
CC arch/arm/kernel/asm-offsets.s
GEN include/generated/asm-offsets.h
CALL scripts/checksyscalls.sh
CC scripts/mod/devicetable-offsets.s
GEN scripts/mod/devicetable-offsets.h
HOSTCC scripts/mod/file2alias.o
HOSTLD scripts/mod/modpost
CC init/main.o
CHK include/generated/compile.h
UPD include/generated/compile.h
CC init/version.o
CC init/do_mounts.o
CC init/do_mounts_initrd.o
LD init/mounts.o
init/do_mounts_initrd.o: In function `return_address':
/opt/keystone-linux-linux/arch/arm/include/asm/ftrace.h:51: multiple definition of `return_address'
init/do_mounts.o:/opt/keystone-linux-linux/arch/arm/include/asm/ftrace.h:51: first defined here
scripts/Makefile.build:441: recipe for target 'init/mounts.o' failed
make[1]: *** [init/mounts.o] Error 1
Makefile:797: recipe for target 'init' failed
make: *** [init] Error 2

Note that I cannot run git from Linux behind my employer's firewall so downloaded the tree as a tgz file from https://git.ti.com/.

Thanks,
John