This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Help! About TSCH and TSCL of C6678?

Hello,I'm using TSCH and TSCL to delay the 5 billion cycles,there will be an error about 1 billion cycles,should be the first to read TSCL,then read TSCH carry occurs when abnormal. Will TSCH and TSCL address is the number? Continuous address it? It can be read simultaneously using these two do? Or there are other solutions?