This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Component responsible for Scan rate conversion

Hi All,


In DM8148 HDVPSS userguide below feature is mentioned.

"Scan rate conversion (up to 1080p 60Hz) is supported to handle video contents with various scan
rates. It can be done via frame/field repeating/skipping."

This feature is highlighted as in general feature of HDVPSS. There is not detailed description given regarding this.

I would like to know which component is responsible for this scan rate conversion.

Thanks,

Jemish