root@am:/opt/ti/ti-processor-sdk-linux-k2l-evm-03.00.00.04/example-applications/openmpacc-examples-1.3.2.0/printf_debug# make
clacc -v -k --hc="-O3 -Wall -Wextra -fopenmp" --tc="-O3" printf_debug_main.o printf_debug_target.c -o printf_debug
>> DEBUG: Extra host compiler options: -O3 -Wall -Wextra -fopenmp
>> DEBUG: Extra target compiler options: -O3
>> DEBUG: Executable binary name: printf_debug
>> DEBUG: Input files: printf_debug_main.o printf_debug_target.c
>> DEBUG: ARM object file or archive: printf_debug_main.o
>> DEBUG: Source code file: printf_debug_target.c
>> DEBUG: Using /opt/ti/ti-processor-sdk-linux-k2l-evm-03.00.00.04/linux-devkit/sysroots/x86_64-arago-linux/usr/bin/arm-linux-gnueabihf-gcc for HOST compilation.
>> DEBUG: Using /opt/ti/ti-processor-sdk-linux-k2l-evm-03.00.00.04/linux-devkit/sysroots/x86_64-arago-linux/usr/bin/arm-linux-gnueabihf-g++ for HOST compilation.
>> DEBUG: Using /opt/ti/ti-processor-sdk-linux-k2l-evm-03.00.00.04/linux-devkit/sysroots/x86_64-arago-linux/usr/bin/cl6x for TARGET compilation.
>> DEBUG: Using /opt/ti/ti-processor-sdk-linux-k2l-evm-03.00.00.04/linux-devkit/sysroots/x86_64-arago-linux/usr/bin/cl6x for S2S compilation.
>> DEBUG: Using /opt/ti/ti-processor-sdk-linux-k2l-evm-03.00.00.04/linux-devkit/sysroots/x86_64-arago-linux/usr/bin/clocl for TARGET compilation.
cl6x --openmp:host -pds=1173 -I/opt/ti/ti-processor-sdk-linux-k2l-evm-03.00.00.04/targetNFS/usr/include -I/opt/ti/ti-processor-sdk-linux-k2l-evm-03.00.00.04/linux-devkit/sysroots/x86_64-arago-linux/ -I/opt/ti/ti-processor-sdk-linux-k2l-evm-03.00.00.04/linux-devkit/sysroots/x86_64-arago-linux/usr/bin/../lib/gcc/arm-linux-gnueabihf/5.3.1/include -I/opt/ti/ti-processor-sdk-linux-k2l-evm-03.00.00.04/linux-devkit/sysroots/x86_64-arago-linux/usr/bin/../lib/gcc/arm-linux-gnueabihf/5.3.1/include-fixed -I/opt/ti/ti-processor-sdk-linux-k2l-evm-03.00.00.04/linux-devkit/sysroots/x86_64-arago-linux/usr/bin/../lib/gcc/arm-linux-gnueabihf/5.3.1/../../../../arm-linux-gnueabihf/include -I/opt/ti/ti-processor-sdk-linux-k2l-evm-03.00.00.04/linux-devkit/sysroots/x86_64-arago-linux/usr/bin/../arm-linux-gnueabihf/libc/usr/include printf_debug_target.c
cl6x --openmp:device -mv6600 -I/opt/ti/ti-processor-sdk-linux-k2l-evm-03.00.00.04/targetNFS/include -I/opt/ti/ti-processor-sdk-linux-k2l-evm-03.00.00.04/targetNFS/usr/share/ti/openmpacc/dsp/include -O3 printf_debug_target.c
"/opt/ti/ti-processor-sdk-linux-k2l-evm-03.00.00.04/targetNFS/usr/share/ti/openmpacc/dsp/include/omp.h", line 42: fatal error: cannot open source file "stdint.h"
1 catastrophic error detected in the compilation of "printf_debug_target.c".
Compilation terminated.
>> Compilation failure
>> ERROR: Target compilation of printf_debug_target.c failed.
make: *** [printf_debug] Error 1
It is impossible to execute a TI software unless you have errors. The above is another one. What should i do?