Hi there, are there any eval board that connects to a peripheral using UPP IF?
I would like to get the hardware reference design for this UPP IF. Thanks
Regards,
Mitesh
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Titus,
Thanks for your reply. I couldn't find any reference design of UPP on OMAP-L138 EVAL board, it looks it's using Video IF.
I am interested to know if there is a need to have a series resister of 22ohm on each of the output pin. Thanks.
Hi Mitesh,
The nominal impedance of the UPP buffers for the OMAP-L138 is 40 ohms. An initial value for the series termination can be selected but simulation of your PCB would result in the best value for your system.
Regards,
Bill
Hi Bill, thanks for the info. Did to get this number from datasheet? is that same for C6748 GPIO pins?
Is this the reason that there is a 22 Ohm resistor on almost all GPIO pin on EVM C6747 as series termination?
thanks.
Hi Mitesh,
I checked the internal specification for the IO cell used on the OMAP part you were asking about. I don't know if the same cell was used on the C6748. Is that the part you are interested in?
Regards,
Bill