Other Parts Discussed in Thread: TDA2
Hi,
I want to enable 6 channels on TDA2xx.
My Vision SDK version is v2.08 and running Linux on A15.
Now, channel 1, 2, 3, 4, 6 are enabled. But channel 5 still can not work.
I did following steps to enable channel 5:
1. Disable NDK in Rules.make
2. Set VIDEO_SENSOR_NUM_LVDS_CAMERAS as 6 in "vision_sdk\examples\tda2xx\include\video_sensor.h"
3. Set pinmux as following:
|
Signal Name from CAMERA |
Signal used on TDA2 |
|
CAM5_D[2] |
VIN4B_D0 (U4) |
|
CAM5_D[3] |
VIN4B_D1 (V2) |
|
CAM5_D[4] |
VIN4B_D2 (Y1) |
|
CAM5_D[5] |
VIN4B_D3 (W9) |
|
CAM5_D[6] |
VIN4B_D4 (V9) |
|
CAM5_D[7] |
VIN4B_D5 (U5) |
|
CAM5_D[8] |
VIN4B_D6 (V5) |
|
CAM5_D[9] |
VIN4B_D7 (V4) |
|
CAM5_HSYNC |
VIN4B_HSYNC1 (U7) |
|
CAM5_VSYNC |
VIN4B_VSYNC1 (V6) |
|
CAM5_PCLK |
VIN4B_CLK1(V1) |
Is there anything I missed to enable the 5th VIP port?
Thanks,
Kevin