Hi Guys,
I have two custom boards, CUSTOM A Board[DM385] & CUSTOM B Board[ LAN9500(PHY input to USB output )].
From CUSTOM B board i will be getting Ethernet to USB converter. USB will be plugged into CUSTOM A board and it need to detect ethernet interface.
question:
1-> What are necessary USB config parameter i have to enable in CUSTOM A Board kernel to support above scenario?
thanks & regards,
Ganesh