Other Parts Discussed in Thread: CC1310
Hi All
When I create a timer from the available products in the configurator I can see the code is added in the cfg.
I would like to run the timer as a one shot.
What I want to do is create a task that executes every so often then when the task executes it must start my one shot timer, When the timer expires it should then toggle a pin.
Now my question, Do I use hardware timer for this if so, how? Or do I use the Timer module from the products.... I struggle to find some documentation on this
Kind regards
Ben
Here my main, where can I get the handle for timer0 that was created in the cfg file?
/*
* Copyright (c) 2015-2016, Texas Instruments Incorporated
* All rights reserved.
*
* Redistribution and use in source and binary forms, with or without
* modification, are permitted provided that the following conditions
* are met:
*
* * Redistributions of source code must retain the above copyright
* notice, this list of conditions and the following disclaimer.
*
* * Redistributions in binary form must reproduce the above copyright
* notice, this list of conditions and the following disclaimer in the
* documentation and/or other materials provided with the distribution.
*
* * Neither the name of Texas Instruments Incorporated nor the names of
* its contributors may be used to endorse or promote products derived
* from this software without specific prior written permission.
*
* THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
* AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
* THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
* PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
* CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
* EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
* PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
* OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
* WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
* OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
* EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
*/
/*
* ======== empty.c ========
*/
/* XDCtools Header files */
#include <xdc/std.h>
#include <xdc/runtime/System.h>
/* BIOS Header files */
#include <ti/sysbios/BIOS.h>
#include <ti/sysbios/knl/Clock.h>
#include <ti/sysbios/knl/Task.h>
/* TI-RTOS Header files */
// #include <ti/drivers/I2C.h>
#include <ti/drivers/PIN.h>
// #include <ti/drivers/SPI.h>
// #include <ti/drivers/UART.h>
// #include <ti/drivers/Watchdog.h>
/* Board Header files */
#include "Board.h"
#define TASKSTACKSIZE 512
Task_Struct task0Struct;
Char task0Stack[TASKSTACKSIZE];
Task_Struct task2Struct;
Char task2Stack[TASKSTACKSIZE];
Task_Struct task1Struct;
Char task1Stack[TASKSTACKSIZE];
/* Pin driver handle */
static PIN_Handle ledPinHandle;
static PIN_State ledPinState;
uint8_t g_configPinStatus=0;
uint8_t g_currentState=0;
/*
* Application LED pin configuration table:
* - All LEDs board LEDs are off.
*/
PIN_Config ledPinTable[] = {
Board_LED0 | PIN_GPIO_OUTPUT_EN | PIN_GPIO_LOW | PIN_PUSHPULL | PIN_DRVSTR_MAX,
Board_LED1 | PIN_GPIO_OUTPUT_EN | PIN_GPIO_LOW | PIN_PUSHPULL | PIN_DRVSTR_MAX,
Board_LED2 | PIN_GPIO_OUTPUT_EN | PIN_GPIO_LOW | PIN_PUSHPULL | PIN_DRVSTR_MAX,
Board_LED3 | PIN_GPIO_OUTPUT_EN | PIN_GPIO_LOW | PIN_PUSHPULL | PIN_DRVSTR_MAX,
PIN_TERMINATE
};
/*
* ======== heartBeatFxn ========
* Toggle the Board_LED0. The Task_sleep is determined by arg0 which
* is configured for the heartBeat Task instance.
*/
Void heartBeatFxn(UArg arg0, UArg arg1)
{
while (1) {
Task_sleep((UInt)arg0);
PIN_setOutputValue(ledPinHandle, Board_LED0,
!PIN_getOutputValue(Board_LED0));
System_printf("Now In hearBeat");
}
}
/*
* ======== LedOffTmr0 ========
* Switch off LED after time out
*/
Void LedOffTmr0(void)
{
PIN_setOutputValue(ledPinHandle, TeqconRadioLedState,0);
}
/*
* ======== StatusLedOnTask ========
* Switch Status LED On
*/
Void LedOnTsk (UArg arg0, UArg arg1)
{
Task_sleep((UInt)arg0);
PIN_setOutputValue(ledPinHandle, TeqconRadioLedState,1);
Timer_start(timer0);
}
/*
* ======== CheckCfgPin ========
* Check Cfg Pin
*/
Void checkCFGPin(UArg arg0, UArg arg1)
{
while (1)
{
Task_sleep((UInt)arg0);
g_configPinStatus = PIN_getInputValue(EnableConfig);
System_printf("Now in checkCfg");
if(g_configPinStatus&1 == 1)
{
PIN_setOutputValue(ledPinHandle, Board_LED2,
!PIN_getOutputValue(Board_LED2));
}
else
{
PIN_setOutputValue(ledPinHandle, Board_LED2,0);
}
}
}
/*
* ======== main ========
*/
int main(void)
{
Task_Params taskParams;
Task_Params cfgChkTsk;
Task_Params ledOffTsk;
/* Call board init functions */
Board_initGeneral();
// Board_initI2C();
// Board_initSPI();
// Board_initUART();
// Board_initWatchdog();
/* Construct heartBeat Task thread */
Task_Params_init(&taskParams);
taskParams.arg0 = 1000000 / Clock_tickPeriod;
taskParams.stackSize = TASKSTACKSIZE;
taskParams.stack = &task0Stack;
Task_construct(&task0Struct, (Task_FuncPtr)heartBeatFxn, &taskParams, NULL);
//task to check for cfg pin
Task_Params_init(&cfgChkTsk);
cfgChkTsk.arg0 = 5000000 / Clock_tickPeriod;
cfgChkTsk.stackSize = TASKSTACKSIZE;
cfgChkTsk.stack = &task1Stack;
Task_construct(&task1Struct, (Task_FuncPtr)checkCFGPin, &cfgChkTsk, NULL);
//task to check for status set pin
Task_Params_init(&ledOffTsk);
ledOffTsk.arg0 = 100000 / Clock_tickPeriod;
ledOffTsk.stackSize = TASKSTACKSIZE;
ledOffTsk.stack = &task2Stack;
Task_construct(&task2Struct, (Task_FuncPtr)checkCFGPin, &cfgChkTsk, NULL);
/* Open LED pins */
ledPinHandle = PIN_open(&ledPinState, ledPinTable);
if(!ledPinHandle) {
System_abort("Error initializing board LED pins\n");
}
//PIN_setOutputValue(ledPinHandle, Board_LED1, 1);
System_printf("Starting the example\nSystem provider is set to SysMin. "
"Halt the target to view any SysMin contents in ROV.\n");
/* SysMin will only print to the console when you call flush or exit */
System_flush();
/* Start BIOS */
BIOS_start();
return (0);
}