boot command stops with the following message, How to boot from USB device:
=> boot
load - load binary file from a filesystem
Usage:
load <interface> [<dev[:part]> [<addr> [<filename> [bytes [pos]]]]]
- Load binary file 'filename' from partition 'part' on device
type 'interface' instance 'dev' to address 'addr' in memory.
'bytes' gives the size to load in bytes.
If 'bytes' is 0 or omitted, the file is read until the end.
'pos' gives the file byte position to start reading from.
If 'pos' is 0 or omitted, the file is read from the start.
=> printenv
addr_mon=0x0c140000
addr_secdb_key=0xc000000
addr_ubi=0x82000000
addr_uinitrd=-
arch=arm
args_all=setenv bootargs console=ttyS0,115200n8 rootwait
args_net=setenv bootargs ${bootargs} rootfstype=nfs root=/dev/nfs rw nfsroot=${serverip}:${nfs_root},${nfs_options} ip=dhcp
args_ramfs=setenv bootargs ${bootargs} rdinit=/sbin/init rw root=/dev/ram0 initrd=0x808080000,80M
args_ubi=setenv bootargs ${bootargs} rootfstype=ubifs root=ubi0:rootfs rootflags=sync rw ubi.mtd=ubifs,4096
args_usb=setenv bootargs ${bootargs} rootfstype=ext4 root=/dev/sda2 rw ip=dhcp
baudrate=115200
board=ks2_evm
board_name=ks2_evm
boot=usb
bootargs=console=ttyS0,115200n8 rootwait rootfstype=ext4 root=/dev/sda2 rw ip=dhcp
bootcmd=run init_${boot} init_fw_rd_${boot} get_fdt_${boot} get_mon_${boot} get_kern_${boot} run_mon run_kern
bootdelay=2
bootdir=/boot
bootm_size=0x10000000
burn_ubi=nand erase.part ubifs; nand write ${addr_ubi} ubifs ${filesize}
burn_uboot_nand=nand erase 0 0x100000; nand write ${loadaddr} 0 ${filesize}
burn_uboot_spi=sf probe; sf erase 0 0x90000; sf write ${loadaddr} 0 ${filesize}
cpu=armv7
fdt_addr_r=0x88000000
fdtaddr=0x88000000
get_fdt_net=dhcp ${fdtaddr} ${tftp_root}/${name_fdt}
get_fdt_nfs=nfs ${fdtaddr} ${nfs_root}/boot/${name_fdt}
get_fdt_ramfs=dhcp ${fdtaddr} ${tftp_root}/${name_fdt}
get_fdt_ubi=ubifsload ${fdtaddr} ${bootdir}/${name_fdt}
get_fdt_usb=load usb 0:1 ${addr_fdt} ${name_fdt}
get_fs_ramfs=dhcp ${rdaddr} ${tftp_root}/${name_fs}
get_kern_net=dhcp ${loadaddr} ${tftp_root}/${name_kern}
get_kern_nfs=nfs ${loadaddr} ${nfs_root}/boot/${name_kern}
get_kern_ramfs=dhcp ${loadaddr} ${tftp_root}/${name_kern}
get_kern_ubi=ubifsload ${loadaddr} ${bootdir}/${name_kern}
get_kern_usb=load usb 0:1 ${addr_kern} ${name_kern}
get_mon_net=dhcp ${addr_mon} ${tftp_root}/${name_mon}
get_mon_nfs=nfs ${addr_mon} ${nfs_root}/boot/${name_mon}
get_mon_ramfs=dhcp ${addr_mon} ${tftp_root}/${name_mon}
get_mon_ubi=ubifsload ${addr_mon} ${bootdir}/${name_mon}
get_mon_usb=load usb 0:1 ${addr_mon} ${name_mon}
get_ubi_net=dhcp ${addr_ubi} ${tftp_root}/${name_ubi}
get_ubi_nfs=nfs ${addr_ubi} ${nfs_root}/boot/${name_ubi}
get_uboot_net=dhcp ${loadaddr} ${tftp_root}/${name_uboot}
get_uboot_nfs=nfs ${loadaddr} ${nfs_root}/boot/${name_uboot}
init_fw_rd_net=dhcp ${rdaddr} ${tftp_root}/${name_fw_rd}; run set_rd_spec
init_fw_rd_ramfs=setenv rd_spec -
init_fw_rd_ubi=ubifsload ${rdaddr} ${bootdir}/${name_fw_rd}; run set_rd_spec
init_fw_rd_usb=setenv rd_spec -
init_net=run args_all args_net
init_nfs=setenv autoload no; dhcp; run args_all args_net
init_ramfs=run args_all args_ramfs get_fs_ramfs
init_ubi=run args_all args_ubi; ubi part ubifs; ubifsmount ubi:rootfs;
init_usb=usb start; run set_fs_none args_all args_usb
kernel_addr_r=0x82000000
loadaddr=0x82000000
mem_lpae=1
mem_reserve=1536M
mtdparts=mtdparts=davinci_nand.0:1024k(bootloader)ro,512k(params)ro,-(ubifs)
name_fdt=keystone-k2l-evm.dtb
name_fs=arago-console-image-k2l-evm.cpio.gz
name_fw_rd=k2-fw-initrd.cpio.gz
name_kern=zImage
name_mon=skern-k2l.bin
name_ubi=k2l-evm-ubifs.ubi
name_uboot=u-boot-spi-k2l-evm.gph
nfs_options=v3,tcp,rsize=4096,wsize=4096
nfs_root=/export
no_post=1
pxefile_addr_r=0x80100000
ramdisk_addr_r=0x88080000
rd_spec=-
rdaddr=0x88080000
run_kern=bootz ${loadaddr} ${rd_spec} ${fdtaddr}
run_mon=mon_install ${addr_mon}
scriptaddr=0x80000000
set_fs_none=setenv addr_uinitrd -
set_rd_spec=setenv rd_spec ${rdaddr}:${filesize}
soc=keystone
tftp_root=/
vendor=ti