Other Parts Discussed in Thread: TMS320VC5505
Hi, I'm running A TMS320VC5505 off of a 12MHz external clock. I realize that the 5505 needs to be powered up in a sequence with the core voltages coming up first and the peripheral and bus voltages coming up second as described in I can't find any place in the datasheet that decribes the timing of how these should come up on power up. Is there any timing? In section 6.3.1 it says that I have to wait until the the core supplies reach .9V I cant exceed a voltage of 1.65V... Is this the only requirement?