This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM36x - NAND: backup and restore NAND?



Any input you can provide on the below?

I want to do a backup of the flash of the daVinci DM36x board, by means of the UART. I'm looking for the right commands to send from UART (nand mode or bootme mode) in order to do a full backup of the flash. I can also use Linux commands, if there is no external tool for this scope. I use sfh_DM36x.exe to write the memory in bootme mode, but it can not perform a backup of the memory. I wish to perform a full backup of the flash in the actual state, before to do any modification.

A.