Other Parts Discussed in Thread: OMAP-L138, OMAPL138
Hi,
I have a question about using omap l138 and c6748. I have Zoom™ OMAP-L138 EVM Development Kit. There are two soms one with omap and one with c6748 on it. Is it possible to run those two processors at the same time (assuming that I have a board that can have those two soms attached at the same time). So that arm could wake up dsp procesor which is in omap or the other one dsp (stand alone c6748 from the other som).