This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Pru hardware serial port uart0 of 3 m baud rate is not accurate

Other Parts Discussed in Thread: AM3358

hi!
     I use board is beagleboneblack, use pru real-time serial port and the fpga communication, but in the "192 - MHZ UART Input Clock and 16 x Over - from Mode" of the baud rate is set to 3 M, but shows the messy  code;When I set the baud rate of 1 M data is correct.My data book on the Table in am3358 part 4-23 detected the Baud Rate corresponding to the Actual Baud Rate value, but didn't find 3 M's Actual Baud Rate, but could not find the Actual Baud Rate and the set value of the corresponding transformation relationship.
I hope you can for pru real-time 3 m of the serial port Baud Rate is given a corresponding Actual Baud Rate!

thank you!!!