Other Parts Discussed in Thread: RFSDK
Hi As per the following thread

It has been mentioned that MBMS feature can be achieved by having 3 different Symbol Indices LUT for Normal Frame, MBMS Frame 1 and Frame 2.
I assume that all these frames would have the same number of samples in 10ms frame ( 3072000) for a 20 MHz case.
My question is can I configure 3 different frames with different frame sizes and at run time choose which frame to receive. For example
Frame 1 = 3072000 samples
Frame 2 = 3072001 samples
Frame 3 = 3071999 samples.
Is there a way in which frame configuration to be received can be changed on FLY
Best regards
LN