This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

VOUT3 port of AM5725

Hi

In our custom Design we are using 24 bit RGB of VOUT3 port  for Encoder . According to silicon errata we have given option for on VDDSHV 6 for 1.8V as well as 3.3V. at the starting we are trying on vddshv6 at 3.3v. We are not able to detect I2c address we can not write on i2c but we are able to read on I2c . we then try on vddshv 1.8 volts but did not work . We again switch to 3.3v after that our debugging UART is not working something is coming but we are unable to write . 

Any suggestion ? any body from TI can help to resolve this issue .

DSP is booting as we are able to display on HDMI.

Regards

Neelam