This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

about "SSC" of "AM335x"



Hello,
I have a question about "SSC" of "AM335x".
"AM335x" incorporates SSCG, but the explanation has a vague point.
There is a register for the setting to use it for "MPU,DDR,CORE,PER".
for example
 8-90. CM_SSC_DELTAMSTEP_DPLL_MPU Register
 8-95. CM_SSC_DELTAMSTEP_DPLL_DDR Register
 8-105.CM_SSC_DELTAMSTEP_DPLL_CORE Register
 8-110.CM_SSC_DELTAMSTEP_DPLL_PER Register
 etc.

It is written for the "NOTE:" that only "LCD,MPU" is usable.
Even if the register exists , but not implemented as a function of "SSC"?
Or is it the mistake of mention?

"SPRUH73N(October 2011 Revised June 2016)"
8.1.6.6 Spread Spectrum Clocking (SSC)
  SSC can be enabled/disabled using bit CM_CLKMODE_DPLL_xxx.DPLL_SSC_EN (where xxx can be
  any one of the following DPLLs: MPU, DDR, DISP, CORE, PER).

  NOTE:Spread spectrum clock is only supported for the LCD and MPU PLLs on this device.
       Spread spectrum clocking is not supported for DDR, PER, DISP, and CORE PLLs.

Best regards , Isao