This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Select which of the two Sitara Processor - AM

Hello All,

I have to analyze the data of a detector with 1000 X 256 pixel size and display the image on LCD.

The LCD specs are:

Size: 7.02 inch

Resolution: 1200(RGB) x1920

Interface: MIPI

I have gone through the details of AM437x and AM335x Sitara series processor details, none of them support MIPI interface. I refered few forums, which says to use CSI/DSI bridge ICs for same.

Can anybody pls suggest which processor and bridge ICs are suitable for my application.

Regards,

Thankyou,

Dhara