Other Parts Discussed in Thread: CC2564
Hi,
Our customer is considering to use CC2564 + AM335x with Linux. They are referring instruction document which is described in below.
http://processors.wiki.ti.com/index.php/Using_CC2564_with_Linux
It mentioned that following three software are required.
(1) Linux EZSDK7.0
(2) LINUXEZSDK-WILINK8-BT
(3) Patch file
Regarding (2), LINUXEZSDK-WILINK8-BT is not available on TI web. Instead, TI-BT-STACK_LINUX-ADDON is available. We guess that this can not work with EZSDK7.0, but we need some modification.
About (3), we need patch file to use Wilinlk8 stack with CC25xx. We can download "ti-sdk-am335x-evm-07.00.00.00-rfcape-cc2564-v0.4.tar", but it is targeted to EZSDK7.0.
In summary, the software which is described on Wiki page are different from actual software which we can download.
================
(a) Can we use TI-BT-STACK_LINUX-ADDON with patch file?
(b If above answer is "no", then can we have LINUXEZSDK-WILINK8-BT?
Regards,
Fukui