I am planning to use MAC ID of AM352 as a serial number for my product.
Each AM3352 Chip has some unique MAC ID pre programmed. And so I will be able to use them to uniquely identify each device.
But, the MAC IDs are of 8 bytes width and so, I am using all these to specify the serial number.
I can avoid using few bytes that are going to be same across all AM3352 chips. Can someone please comment on the above and if possible give the range of MAC IDs that are planned to be used for AM3352.
Thanks in advance.
~Raja