Hi Champs,
I would like to realize total 64 mic input on AM335x with Linux OS.
Actually, AM335x has 2 McASP. but, there is each 4serial input only.
However, each of McASP maximum 32 TDM slot. If we use 8ch ADC and TDM output or I2S,
this total 8ch ADC * 4 serial port *2McASP =64.
Is it correct ? But, I think 8ch ADC and TDM out put is expensive. So, do you have another idea to realize 64 microphone input.
Regards,
Kz777