Other Parts Discussed in Thread: DM385, TVP5158
Hi TI Experts,
I'm in customized DM385 platform. IPNC RDK 3.5
Using TVP5158 decoder getting 4CH @ D1resolution.
CaptureLink_CreateParams_Init(&capturePrm);
capturePrm.numVipInst = 1;
capturePrm.tilerEnable = FALSE;
capturePrm.numBufsPerCh = 10;
capturePrm.fakeHdMode = FALSE;
capturePrm.enableSdCrop = FALSE;
capturePrm.doCropInCapture = FALSE;
pCaptureInstPrm = &capturePrm.vipInst[0];
pCaptureInstPrm->vipInstId = SYSTEM_CAPTURE_INST_VIP1_PORTA;
pCaptureInstPrm->videoDecoderId = SYSTEM_DEVICE_VID_DEC_TVP5158_DRV;
pCaptureInstPrm->standard = SYSTEM_STD_MUX_4CH_D1;
pCaptureInstPrm->numOutput = 1;
pCaptureInstPrm->inDataFormat = SYSTEM_DF_YUV422P;
pCaptureOutPrm = &pCaptureInstPrm->outParams[0];
pCaptureOutPrm->dataFormat = SYSTEM_DF_YUV422I_YUYV;
pCaptureOutPrm->scEnable = FALSE;
pCaptureOutPrm->scOutWidth = 0;
pCaptureOutPrm->scOutHeight = 0;
pCaptureOutPrm->outQueId = 0;
Able to see only one stream...,
After capture using Deinterlacer and scaler and display link (CAP --> DEI --> SCLR --> DIS)
If I changed the display channel number in display link, I could able to see the individual stream
But I want to change the display in dynamic using systemlinkcontrol API (Or is it required to demux other streams from an Usecase file ???)
I tried to change the channel using SetchannelSwitch() and calling VdisSwitchActive channel but it is not effecting our side !!!
How I can switch the channel from one decoder ???
Kindly suggest me to solve this issue ???
Regards,
Rajesh Kannan.S