This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM335x GPMC reconfiguration



Our customer wants to reconfigure GPMC in an interval between accesses. How can this be implemented?

Section 7.1.2.3.8.1 on TRM (SPRUH73N) describes:

 "Chip-select configuration (base and mask address or any protocol and timing settings) must be performed
  while the associated chip-select is disabled through the GPMC_CONFIG7_i[6] CSVALID bit. In addition, a
  chip-select configuration can only be disabled if there is no ongoing access to that chip-select. This
  requires activity monitoring of the prefetch or write-posting engine if the engine is active on the chip-select.
  Also, the write buffer state must be monitored to wait for any posted write completion to the chip-select."

It requires to monitor the write buffer state, the prefetch or write-posting engine activity state. Which are fields in the registers indicating each state?

Best regards,

Daisuke