This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM365: How to set USB_VBUS pin.



Hi,

I am working on a DM365 based customize board on which a USB hub chip is used. As per DM365 datasheet the USB connector power must be turned on by the DM365, when th DM365 is the host. Also the pin N2 called USB_VBUS on the DM365 is responsible to USB power enable on the USB hub. I want to verify how the pin is configured in the kernel that I am using (linux-2.6.18_pro500). I want to set this pin as HIGH. Can anyone tell me how can I do this in kernel? Is it possible through UBoot? 

Thanks in advance!!!

--
Regards,
Krunal Patil