Hi there
I have a question about the schematic of TMSDSLCDK6748
I'm looking "C6748 LC DEV KIT VER A7E.pdf"
page7 of the "C6748 LC DEV KIT VER A7E.pdf"
Description of the P17 is written as "VPIF_DIN8/UHPI_HD0/UPP_CH1_D0/GPIO8[6]"
it means that P17 Could Work not only as Databus[0] of the UPP and also GPIO8[7]
But, in the TMS320C6748 Datasheet(page 23)
A pin which could work as Databus[0] is also could configured as GPIO6[5]
Do you have any idea?
i attached some picture for you
One more thing
CH1 of the Description of the P17 ("VPIF_DIN8/UHPI_HD0/UPP_CH1_D0/GPIO8[6]")
Meaing what?