Dear Community,
I am trying to build SDK [1] from the developer guide and getting following error. Could you check if this real issue? I think it is because "https://cpuset.googlecode.com/files/cpuset-1.5.6.tar.gz"
NOTE: Preparing RunQueue
NOTE: Executing SetScene Tasks
NOTE: Executing RunQueue Tasks
WARNING: cpuset-1.5.6-r0 do_fetch: Failed to fetch URL cpuset.googlecode.com/.../cpuset-1.5.6.tar.gz, attempting MIRRORS if available
ERROR: cpuset-1.5.6-r0 do_fetch: Fetcher failure: Fetch command failed with exit code 8, output:
cpuset.googlecode.com/.../cpuset-1.5.6.tar.gz:
2016-09-02 14:43:48 ERROR 404: Not Found.
ERROR: cpuset-1.5.6-r0 do_fetch: Function failed: Fetcher failure for URL: 'cpuset.googlecode.com/.../cpuset-1.5.6.tar.gz'. Unable to fetch URL from any source.
ERROR: Logfile of failure stored in: /home/work/ti_sdk_dra7xx/yocto-layers/build/arago-tmp-external-linaro-toolchain/work/cortexa15hf-neon-linux-gnueabi/cpuset/1.5.6-r0/temp/log.do_fetch.9197
ERROR: Task 1810 (/home/work/ti_sdk_dra7xx/yocto-layers/sources/meta-arago/meta-arago-extras/recipes-support/cpuset/cpuset_1.5.6.bb, do_fetch) failed with exit code '1'
NOTE: Tasks Summary: Attempted 3246 tasks of which 3243 didn't need to be rerun and 1 failed.
NOTE: Writing buildhistory
Waiting for 0 running tasks to finish:
Summary: 1 task failed:
/home/work/ti_sdk_dra7xx/yocto-layers/sources/meta-arago/meta-arago-extras/recipes-support/cpuset/cpuset_1.5.6.bb, do_fetch
Summary: There were 2 WARNING messages shown.
Summary: There were 2 ERROR messages shown, returning a non-zero exit code.
[PSDKLA]>
[PSDKLA]> Completed Yocto build at Fri Sep 2 14:44:17 IST 2016
[PSDKLA]>
user1@linux1:~/work/ti_sdk_dra7xx/yocto-layers$
Thanks & Regards,
Vikash