Other Parts Discussed in Thread: AM3352
Sitara Team,
We just received a call from our customer. They are testing their AM3352 board with 16.5KV (Air Gap) and seeing failures on the AM3352 Touch Screen Inputs. We reviewed the design below and the ESD devices they are using.
ESD Device – Schematic shows 5V bidirectional device from AVX. They have switched to 3.3V bidirectional device with no better results.
Part Number is VC060303A100DP
http://datasheets.avx.com/tguard.pdf
They have also replaced the zero ohm jumpers in the schematic (R1010-R1013) with 600 ohm ferrite inductors.
Part Number BLM18E601SH1D
They would like to increase the capacitance shown on the touch screen interface but needs to figure out the limitation of the ADC input. A quick look at the AM3352 Datasheet and TRM shows this is not a trivial question. The touch screen inputs are highly programmable and it is unclear how the device operates and what the impedances are in the touch screen mode. We'd, therefore, like to reach out on the Forums for more guidance.
We’ll be looking at this closer myself and would like to reach back out this afternoon to the customer. Let me know if anyone has any input/guidance?
Thanks!
C. Yorkey (on behalf of customer)