Other Parts Discussed in Thread: CCSTUDIO
Hello Everyone,
I have been attempting to modify the "SpO2_System_v5_0" codebase that ships with the SpO2 AFE board so that it will compile and run on my Spectrum Digital EVM5515.
Whilst trying to figure out how to go about this, I came across a previous thread on this forum in which it was mentioned that a newer version of the codebase ( "SpO2_System_v5_1") has been released for the C5505 eZdsp development tool. I have managed to download the "SpO2.out" file to my EVM5515, and it seems to be running as expected.
What I would like to be able to do now is to compile the codebase. The release notes that ship with the "SpO2_System_v5_1" codebase state that Codegen version 3.36 should be used to build the project, and alas I have been unable to find any mention of this legacy version on the TI website. Could someone please inform me how I can get hold of a copy of this version?
Thanks for any help.
- Rodney