Other Parts Discussed in Thread: TCI6638K2K
Hi,
I'm using TCI6638K2K device and loading Linux on it.
The current problem is that after loading Linux kernel using TFTP in U-Boot and booting, Gigabit Ethernet doesn't work.
It definitely works in U-Boot as I said I loaded kernel via TFTP in U-Boot.
While I'm working on this problem, I found that GbE seems to work when I enable DDR3A_REMAP_EN which was disabled on board circuit in the first place.
So, here's my questions :
1) Is it possbile for DDR3A_REMAP_EN to make difference in Ethernet operation?
2) Can I enable DDR3A_REMAP_EN function during Linux booting even though DDR3A_REMAP_EN was disable in hardware? (for example, configuring device tree file(dts))