This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

sometimes am3354 crash when Uncompressing Linux...

Other Parts Discussed in Thread: AM3354

sometimes am3354 crash when Uncompressing Linux... but most of the reset is ok

the log is followed: and the log stop printing there,I want to use the watchdog to deal with this problem, but I dont kown hown to use it?

Hit any key to stop autoboot:  0 mmc1(part 0) is current device SD/MMC found on device 1 reading uEnv.txt 214 bytes read in 3 ms (69.3 KiB/s) Loaded environment from uEnv.txt Importing environment from mmc ... Running uenvcmd ... reading uImage 4157040 bytes read in 921 ms (4.3 MiB/s) ## Booting kernel from Legacy Image at 81000000 ...    Image Name:   Linux-3.2.0    Image Type:   ARM Linux Kernel Image (uncompressed)    Data Size:    4156976 Bytes = 4 MiB    Load Address: 80008000    Entry Point:  80008000    Verifying Checksum ... OK    Loading Kernel Image ... OK OK

Starting kernel ...

Uncompressing Linux... done, booting the kernel.