This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83848 works with TDA2x DSP

Dear Sir,

According to the TDA2x DSP  reference design it uses DP83865+ TDA2X but this PHY DP83865 is a commercial part (0~70degC), do you have another suggestion  for automotive grade part?

Does DP83848 can work with TDA2X DSP?  Thanks.

  • Dear Sir,
    We have a urgent case need your help to check this communicated issue.


    We have tried to connect TDA2X and DP83848 but we have a problem to communicate both side.
    So far we got this this information below.
    please help check this DP83848 PHY message . Is it functional Or malfunction ?
    Thanks.

    -------------------------------------------------------------------------------------------------------
    [Cortex_M4_IPU1_C0]
    MAC Port 0 Address:
    d0-b5-c2-5b-42-ee

    MAC Port 1 Address:
    d0-b5-c2-5b-42-ef
    GMACSW has been started successfully
    Registration of the GMACSW Successful
    Service Status: DHCPC : Enabled : : 000
    Service Status: Telnet : Enabled : : 000
    Service Status: HTTP : Enabled : : 000
    Service Status: HTTP : Enabled : : 000
    Service Status: DHCPC : Enabled : Running : 000
    PHY: 0, NegMode 01E1, NWAYadvertise 01E1, NWAYREadvertise 43E1
    Negotiated connection: FullDuplex 100 Mbs
    Link Status: 100Mb/s Full Duplex on PHY 0
    <--------wait 50 seconds.....
    Service Status: DHCPC : Enabled : Fault : 002
    <--------hang on this point.
    ------------------------------------------------------------------------------------------------------
  • I moved this to the forums where they support the TDA2x processor; however, you might want to ask this question on the ethernet forums as well to reach the people who support the DP83848.

    e2e.ti.com/.../903
  • Hi,

    The question is submitted to experts.

    Best regards
    Lucy
  • Hello Eason,

    I believe this issue is resolved in another e2e query. If yes can you please mark this as answered.
    e2e.ti.com/.../536720