This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAPL-138 UART Communication Issue

Hi,

    I am using OMAPL-138 package in my project. I configured UART channels on DSP core as per below settings. I am using OMAPL_138_StarterWare_1_10_04_01.

// UART Settings

    PSCModuleControl(SOC_PSC_0_REGS, HW_PSC_UART0, PSC_POWERDOMAIN_ALWAYS_ON,
           PSC_MDCTL_NEXT_ENABLE);
    UARTPinMuxSetup(0, TRUE);

    config = UART_WORDL_8BITS;

    UARTConfigSetExpClk(SOC_UART_0_REGS, SOC_UART_0_MODULE_FREQ,
                            BAUD_115200, config,
                            UART_OVER_SAMP_RATE_16);
    UARTFIFOEnable(SOC_UART_0_REGS);

    UARTFIFOLevelSet(SOC_UART_0_REGS, UART_RX_TRIG_LEVEL_1);

   IntRegister(C674X_MASK_INT6, SCID_SCI0Interrupt_it);
   IntEventMap(C674X_MASK_INT6, SYS_INT_UART0_INT);
   IntEnable(C674X_MASK_INT6);

// Code End

//ISR Routine

unsigned int int_id = 0;

    int_id = UARTIntStatus(SOC_UART_0_REGS);

    IntEventClear(SYS_INT_UART0_INT);


  if(UART_INTID_RX_DATA == int_id)
    {
     while(UARTCharsAvail(SOC_UART_0_REGS))
     {
     rxData[count_rx++] = UARTCharGetNonBlocking(SOC_UART_0_REGS);
     }
    }
 }

Problem:

UART channel is not able to receive complete data from other module. Sometime it's performance is good but not consistently. For example if we send 20 characters from other module on UART, omapL_138 is able to receive only 10 characters(sometime complete data, sometime 12 characters like that) remaining characters are discarded by DSP core.

Please do needful. 

Regards,

Mitul Shinde