HI,
I have made changes according to spraap7.pdf this pdf for compact flash detection in kernel make menuconfig . but still its not getting properly please suggest me. I am using sandisk ultra II 4 gb compact flash . heare i have attached the log also please take a look. and suggest me to how to move forward.
-Boot > nand write 0x80700000 0x60000 0x200000
NAND write: device 0 offset 0x60000, size 0x200000
2097152 bytes written: OK
U-Boot > setenv bootcmd 'nboot 0x80700000 0 0x60000; bootm'
U-Boot > saveenv
Saving Environment to NAND...
Erasing Nand...
Erasing at 0x0 -- 100% complete.
Writing to Nand... done
U-Boot > DM644x_810MHz initialization passed!
TI UBL Version: 1.50
Booting Catalog Boot Loader
BootMode = NAND
Starting NAND Copy...
Valid magicnum, 0xA1ACED66, found in block 0x00000006.
DONE
Jumping to entry point at 0x81080000.
U-Boot 2009.03 (Jun 21 2010 - 16:30:08)
I2C: ready
DRAM: 256 MB
NAND: NAND device: Manufacturer ID: 0xec, Chip ID: 0x36 (Samsung NAND 64MiB 1,8V 8-bit)
64 MiB
In: serial
Out: serial
Err: serial
ARM Clock: 405MHz
DDR Clock: 189MHz
Ethernet PHY: LXT972 @ 0x01
Hit any key to stop autoboot: 0
Loading from NAND 64MiB 1,8V 8-bit, offset 0x60000
Image Name: Linux-2.6.18_pro500-davinci_evm-
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 2017252 Bytes = 1.9 MB
Load Address: 80008000
Entry Point: 80008000
## Booting kernel from Legacy Image at 80700000 ...
Image Name: Linux-2.6.18_pro500-davinci_evm-
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 2017252 Bytes = 1.9 MB
Load Address: 80008000
Entry Point: 80008000
Verifying Checksum ... OK
Loading Kernel Image ... OK
OK
Starting kernel ...
Uncompressing Linux..................................................................................................................................... done, booting the kernel.
Linux version 2.6.18_pro500-davinci_evm-arm_v5t_le (root@yash12) (gcc version 4.2.0 (MontaVista 4.2.0-16.0.32.0801914 2008-08-30)) #1 PREEMPT Thu Sep 1 20:12:36 IST 2016
CPU: ARM926EJ-S [41069265] revision 5 (ARMv5TEJ), cr=00053177
Machine: DaVinci EVM
Memory policy: ECC disabled, Data cache writeback
DaVinci DM6443 variant 0x1
CPU0: D VIVT write-back cache
CPU0: I cache: 16384 bytes, associativity 4, 32 byte lines, 128 sets
CPU0: D cache: 8192 bytes, associativity 4, 32 byte lines, 64 sets
Built 1 zonelists. Total pages: 30208
Kernel command line: video=davincifb:vid0=0,2500K: vid1=0,2500K:osd0=720x576x16,2025K davinci_enc_mngr.ch0_output=COMPOSITE davinci_enc_mngr.ch0_mode=$(videostd) console=ttyS0,115200n8 noinitrd rw ip=192.168.1.103 root=/dev/nfs nfsroot=192.168.1.122:/public/filesys,nolock mem=118M
PID hash table entries: 512 (order: 9, 2048 bytes)
Clock event device timer0_0 configured with caps set: 03
Console: colour dummy device 80x30
Dentry cache hash table entries: 16384 (order: 4, 65536 bytes)
Inode-cache hash table entries: 8192 (order: 3, 32768 bytes)
Memory: 118MB = 118MB total
Memory: 115328KB available (3457K code, 689K data, 172K init)
Security Framework v1.0.0 initialized
Capability LSM initialized
Mount-cache hash table entries: 512
CPU: Testing write buffer coherency: ok
NET: Registered protocol family 16
DaVinci: 71 gpio irqs
WARNING: both IDE and NOR flash are enabled, but share pins.
Disable IDE for NOR support.
ch0 default output "COMPOSITE", mode "NTSC"
MUX: initialized LOEEN
MUX: initialized LFLDEN
VPBE Encoder Initialized
LogicPD encoder initialized
SCSI subsystem initialized
usbcore: registered new driver usbfs
usbcore: registered new driver hub
NET: Registered protocol family 2
IP route cache hash table entries: 1024 (order: 0, 4096 bytes)
TCP established hash table entries: 4096 (order: 2, 16384 bytes)
TCP bind hash table entries: 2048 (order: 1, 8192 bytes)
TCP: Hash tables configured (established 4096 bind 2048)
TCP reno registered
davinci_spi_board_init: NO spi support
VFS: Disk quotas dquot_6.5.1
Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
squashfs: version 3.1 (2006/08/19) Phillip Lougher
JFFS2 version 2.2. (NAND) (C) 2001-2006 Red Hat, Inc.
yaffs Sep 1 2016 20:15:19 Installing.
SGI XFS with no debug enabled
Initializing Cryptographic API
io scheduler noop registered
io scheduler anticipatory registered (default)
LTT : ltt-facilities init
LTT : ltt-facility-core init in kernel
davincifb davincifb: dm_osd0_fb: 720x480x16@0,0 with framebuffer size 675KB
davincifb davincifb: dm_vid0_fb: 0x0x16@0,0 with framebuffer size 2500KB
davincifb davincifb: dm_osd1_fb: 720x480x4@0,0 with framebuffer size 675KB
davincifb davincifb: dm_vid1_fb: 0x0x16@0,0 with framebuffer size 1020KB
davincifb davincifb.0: dm_osd0_fb: Failed to obtain ownership of OSD window.
DAVINCI-WDT: DaVinci Watchdog Timer: heartbeat 60 sec
Serial: 8250/16550 driver $Revision: 1.90 $ 2 ports, IRQ sharing disabled
serial8250.0: ttyS0 at MMIO map 0x1c20000 mem 0xfec20000 (irq = 40) is a 16550A
RAMDISK driver initialized: 1 RAM disks of 32768K size 1024 blocksize
netconsole: not configured, aborting
TI DaVinci EMAC: MAC address is 00:0e:99:02:43:b1
TI DaVinci EMAC Linux version updated 4.0
TI DaVinci EMAC: Installed 1 instances.
Linux video capture interface: v2.00
vpfe vpfe.1: DaVinci v4l2 capture driver V1.0 loaded
Trying to register davinci display video device.
layer=c088d600,layer->video_dev=c088d760
Trying to register davinci display video device.
layer=c088d400,layer->video_dev=c088d560
davinci_init:DaVinci V4L2 Display Driver V1.0 loaded
Davici AEW Driver cannot be loaded
VIDEO PORT is not enabledData Flow path from CCDC is disabled
Davinci AF driver cannot be loaded
VIDEO PORT is not enabled
CCDC needs to be configured<6>i2c /dev entries driver
Uniform Multi-Platform E-IDE driver Revision: 7.00alpha2
ide: Assuming 50MHz system bus speed for PIO modes; override with idebus=xx
MUX: initialized HDIREN
MUX: initialized ATAEN
ide0: MMIO-DMA , BIOS settings: hda:pio, hdb:pio
hda: 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0, ATA DISK drive
ide0 at 0xfec661f0-0xfec661f7,0xfec663f6 on irq 22
hda: max request size: 128KiB
hda: 7928928 sectors (4059 MB) w/2049KiB Cache, CHS=7866/16/63, BUG DMA OFF
hda: task_no_data_intr: status=0x51 { DriveReady SeekComplete Error }
hda: task_no_data_intr: error=0x04 { DriveStatusError }
ide: failed opcode was: 0xef
hda: unknown partition table
Initializing USB Mass Storage driver...
usbcore: registered new driver usb-storage
USB Mass Storage support registered.
usbcore: registered new driver usbhid
drivers/usb/input/hid-core.c: v2.6:USB HID core driver
musb_hdrc: version 6.0, cppi-dma, host, debug=0
musb_hdrc musb_hdrc: No DMA interrupt line
musb_hdrc: USB Host mode controller at c785e000 using DMA, IRQ 12
musb_hdrc musb_hdrc: MUSB HDRC host driver
musb_hdrc musb_hdrc: new USB bus registered, assigned bus number 1
usb usb1: configuration #1 chosen from 1 choice
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
mice: PS/2 mouse device common for all mice
rtc_davinci_evm rtc_davinci_evm: rtc intf: proc
rtc_davinci_evm rtc_davinci_evm: rtc intf: dev (254:0)
rtc_davinci_evm rtc_davinci_evm: rtc core: registered rtc_davinci_evm as rtc0
rtc0: hours 12-23 are misreported as duplicate hours 00-11
davinci-mmc davinci-mmc.0: Supporting 4-bit mode
davinci-mmc davinci-mmc.0: Using DMA mode
Advanced Linux Sound Architecture Driver Version 1.0.12rc1 (Thu Jun 22 13:55:50 2006 UTC).
ASoC version 0.13.1
MUX: initialized MCBSP
AIC3X Audio Codec 0.1
asoc: aic3x <-> davinci-i2s mapping ok
ALSA device list:
#0: DaVinci EVM (aic3x)
IPv4 over IPv4 tunneling driver
TCP bic registered
NET: Registered protocol family 1
NET: Registered protocol family 17
Time: timer0_1 clocksource has been installed.
Clock event device timer0_0 configured with caps set: 08
Switched to high resolution mode on CPU 0
rtc_davinci_evm rtc_davinci_evm: setting the system clock to 2004-02-01 12:16:16 (1075637776)
IP-Config: Guessing netmask 255.255.255.0
IP-Config: Complete:
device=eth0, addr=192.168.1.103, mask=255.255.255.0, gw=255.255.255.255,
host=192.168.1.103, domain=, nis-domain=(none),
bootserver=255.255.255.255, rootserver=192.168.1.122, rootpath=
Looking up port of RPC 100003/2 on 192.168.1.122
Looking up port of RPC 100005/1 on 192.168.1.122
VFS: Mounted root (nfs filesystem).
Freeing init memory: 172K
INIT: version 2.86 booting
Starting the hotplug events dispatcher: udevd.
Synthesizing the initial hotplug events...done.
Waiting for /dev to be fully populated...done.
Activating swap...done.
Remounting root filesystem...done.
Calculating module dependencies
WARNING: Couldn't open directory /lib/modules/2.6.18_pro500-davinci_evm-arm_v5t_le: No such file or directory
FATAL: Could not open /lib/modules/2.6.18_pro500-davinci_evm-arm_v5t_le/modules.dep.temp for writing: No such file or directory
Loading modules:
Checking all file systems: fsck
fsck 1.40 (29-Jun-2007)
Mounting local filesystems: mount nothing was mounted
umount.nfs: /dev/root: not found or not mounted
Setting up networking ....
/etc/network/options is deprecated.
Setting up IP spoofing protection: rp_filter done.
Disabling IPv4 packet forwarding: done.
Disabling TCP/IP Explicit Congestion Notification: done.
Starting network interfaces: done.
Starting hotplug subsystem:
pci
pci [success]
usb
usb [success]
isapnp
isapnp [success]
ide
ide [success]
input
input [success]
scsi
scsi [success]
done.
Starting portmap daemon....
Cleaning: /tmp /var/lock /var/run done.
Updating /etc/motd...done.
INIT: Entering runlevel: 3
Starting system log daemon: syslogd klogd.
Starting NFS common utilities: statd.
Starting internet superserver: inetd.
Starting OpenBSD Secure Shell server: sshd.
MontaVista(R) Linux(R) Professional Edition 5.0.0 (0801921)
192.168.1.103 login: root
Last login: Sun Feb 1 01:05:35 2004 on console
Linux 192.168.1.103 2.6.18_pro500-davinci_evm-arm_v5t_le #1 PREEMPT Thu Sep 1 20:12:36 IST 2016 armv5tejl GNU/Linux
root@192.168.1.103:~# nfs: server 192.168.1.122 not responding, still trying
nfs: server 192.168.1.122 not responding, still trying
ide0: unexpected interrupt, status=0x00, count=1