This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How to reduce the GPMC operating frequency of AM335x

Other Parts Discussed in Thread: AM3352

In My System I have connected TI-DSP 5502 HPI interface with the AM3352 GPMC module.

TI-DSP 5502 HRDY pin is connected with the Wait pin of the AM3352 Processor.

We have configured the GPMC module Chip select 2 with the Asynchronous interface and with Low polarity wait signal.

In normal case the Read and Write operation with the TI-DSP is working fine.

In same case data read by the Processor is not perfect 

So to analysis the issue in more detailed I want to reduce the clock frequency of the the GPMC module.

As mention in the data sheet GMPC clock is CORE_CLKOUTM4/2 

So is there any way I can able to reduce the operating frequency of the GPMC module.

Please provide me the detailed

I am using the uboot: u-boot-2013.01.01

Linux kernal: Kernel-3.14.26

Regards