Hello,
I'm designing a board that will be equipped with an OMAPL138 and a NAND serial FLASH, I'd like to use the boot mode "SPI BOOT" but I'm wondering if a NAND serial FLASH device could be used. On the evaluation module (LOGIC) an SPI NOR flash is mounted, however for design reasons I need to use a NAND serial FLASH but using again the serial SPI protcolo both for booting and for flashing. Is there any solution or application report that considers an SPI boot by using a NAND serial FLASH instead of a SPI NOR FLASH?
Thanks for your time,
Bestr regards,
Giambattista