Folks,
This question of mine is about CC2640, but it's almost identical to this older one about C2000.
I have installed CCStudio 6.1.3 .
I have installed Bluetooth Low Energy SDK. TI-RTOS came with it.
I want to gain in-depth understanding of the TI-RTOS, so I'm following the instruction for Lab 04 in the RTOS training series. The lab manual has this snippet (p.47), which shows that I should select a certain project template when I create a new project.
But my installation of CCStudio and TI-RTOS doesn't have these options.
What am I missing?
Any suggestion, insight or reference is really appreciated!
Cheers,
- Nick