Hello,
I am busy with a project and I am a bit lost at the moment. A bit of background: I am doing a monopulse audio sonar system that uses a speaker and 4 microphones to track a moving target. I am doing range-doppler processing on each channel as well as monopulse processing. The system needs to operate in real time, thus I decided to use the tms320c6657 DSP for the computational power it offers.
The microphones get sampled by an AD7864 ADC chip with simultaneous sampling on all 4 channels. The chip uses a 12 bit parallel port to interface the data to a processor. At the moment, I don't know how to approach this. I have already set up the board and have been able to run example programs like FFT examples etc. However, I am struggling with the setup of the uPP peripheral. What method would you recommend? I want to use the Chip Support Libraries (CSL) but I can't find any decent documentation on this for the c66xx devices. Also, I would prefer not to use SYS/BIOS, only PDK. Can anyone direct me in the direction I need to go to start using the uPP on the board? Any help will really be appreciated.
Kind regards
Wicus